Temperature Logging using internal ADC/TempSensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Temperature Logging using internal ADC/TempSensor

跳至解决方案
2,970 次查看
saipriyasubrama
Contributor II

I am using a S9KEAZ16 controller and would like to use one of the ADC channels as a temp sensor to monitor the CPU temp. The ADC is hardware triggered using a FlexTimer module. I am able to read the measured temperature values on FreeMaster although, I am not able to log it in a data logger.

I am using the EEPROM driver from the blog Driver for Microchip 24xx Serial EEPROM | MCU on Eclipse  and I would like to log the temp sensor reading as and when I receive them. Is it advisable to write the temp sensor values inside the ADC ISR itself? I am worried about the ADC ISR consuming more time to execute and as a result of which a few triggers missed or vice versa incorrect data written on the EEPROM because of lag.

Also is there a way to write float values on my EEPROM?

I tried writing the temp sensor value inside the ADC ISR and the loop gets hung up in the writeblock routine.

do
{
}while(!GI2C1_deviceData.dataTransmittedFlg);

Is there a way to debug this issue??

0 项奖励
回复
1 解答
2,660 次查看
egoodii
Senior Contributor III

For use of the internal temp sense, you should examine my considerations in:

On-chip temperature Calculations 

If you've enabled a full-printf library version, then sprintf is a way to get the system to format an internal float value into a string for you

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,661 次查看
egoodii
Senior Contributor III

For use of the internal temp sense, you should examine my considerations in:

On-chip temperature Calculations 

If you've enabled a full-printf library version, then sprintf is a way to get the system to format an internal float value into a string for you

0 项奖励
回复
2,660 次查看
saipriyasubrama
Contributor II

Thank you. Earl. I figured it out and used Term! component to display my temperature.

0 项奖励
回复