TWR-MEM and TWR-LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,366件の閲覧回数
weblar
Contributor V

Is it at all possible to use both the TWR-MEM and the TWR-LCD modules together in the Tower Stack?

The reason I ask is that the MRAM on the TWR-MEM and the LCD signals appear to share the same pins on the ELEV modules.

I'm wanting to use the MRAM on the TWR-MEM as a frame buffer for the LCD, with a view to supporting displays with higher resolutions (i.e 640x480, 800x600, etc).

Thanks in advance,

Kev

Tower Geeks

ラベル(1)
0 件の賞賛
返信
1 解決策
3,939件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

TWR-LCD also allows access from Tower MCU modules through SPI port, so you may set TWR-LCD controled by SPI and TWR-MEM accessed by FlexBusa1.JPG.

Or you may connect other FB_CSn such as FB_CS1 to J10 pin 2 when it is opened, so that TWR-LCD and TWR-MEM are both attached on flexBus with difference CS signals.

a2.JPG

Hope that helps,

B.R

Kan

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
3,940件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

TWR-LCD also allows access from Tower MCU modules through SPI port, so you may set TWR-LCD controled by SPI and TWR-MEM accessed by FlexBusa1.JPG.

Or you may connect other FB_CSn such as FB_CS1 to J10 pin 2 when it is opened, so that TWR-LCD and TWR-MEM are both attached on flexBus with difference CS signals.

a2.JPG

Hope that helps,

B.R

Kan

0 件の賞賛
返信
3,939件の閲覧回数
weblar
Contributor V

Hi,

Thank you for your reply.

I want to drive the display using the 16bit EBI mode.

Can this be done using the FlexBus peripheral or will I need to change the MUX back to GPIO and drive the pins differently? Either way, I need the swapping between MRAM and the display to be as fast as possible.

Best regards,

K

0 件の賞賛
返信
3,939件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, it can be done with the option of "PS2 - ON PS0 - OFF", and you needn't change the mux to GPIO, just do some modification on hardware, the TWR-LCD is selected by FB_CS0 in 16bit EBI mode, and TWR-MEM is also selected by FB_CS0 at default, but we can connected another CS to it, such as FB_CS2, (FB_CS1 is used as FB_ALE for TWR-MEM). When flexBus is configured, you may let CS0 control TWR-MEM, CS2 control TWR-LCD by mapping them to difference address. We provide bare metal project on FlexBus, please kindly refer to KINETIS512_SC\build\iar\flexbus for details.

BTW, /FB_CS2 can use the pin of PTC18 , providing you are referring to TWR-K60N512, the signal might be difficult to fetch on the  TWR-K60N512

a1.JPG

but can be easily accessed if you using with TWR-SER,

a1.JPG

a1.JPG

In summary, You may build the whole tower system with TWR-K60N512,TWR-SER,TWR-MEM and TWR-LCD, and connect pin 2 of J18 on TWR-SER with  pin 2 of J10 on TWR-MEM. Please kindly refer to the following for details.

a1.JPG

Hope that helps,

B.R

Kan

3,939件の閲覧回数
weblar
Contributor V

Thanks again for your reply.

I will be using the stack with TWR-SER.

I've seen the FlexBus example which makes use of the MRAM chip - this looks quite straightforward to implement. However I'm still not fully certain how I can use the FlexBus to drive the LCD display. You mention mapping the LCD to a different FlexBus address - how would this help me?

Best regards,

K

0 件の賞賛
返信
3,939件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Mapping the LCD to a different FlexBus address just helps TWR-MEM and TWR-LCD have the diffenrent system mapping address so that the application code can read /write to them independently by asserting different FB_CSn signals.


You know, FlexBus has the following memory map:

1.JPG

and TWR-MEM and TWR-LCD share the same flexBus interface except the chip select signal. so you may configure 0x60000000 based address for FB_CS0 and 0x80000000 based address for FB_CS2 , and these two FB_CSx signals control accesses for TWR-MEM and TWR-LCD in the above attached tower system.

Hope that helps,

B.R

Kan

0 件の賞賛
返信
3,939件の閲覧回数
weblar
Contributor V

Thanks for the information - that makes much more sense now.

One final question. I want to use 8080 parallel 16-bit mode to drive a custom display via the FlexBus. The TWR-LCD uses 6800 mode with E and R/W signals whereas 8080 has separate RD and WR signals - how would the FlexBus deal with these?

Best regards,

K

0 件の賞賛
返信
3,939件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Kevin,

There is not a good compatibility between Flexbus and 8080 type bus.

But I know that this is a working configuration with a 8080 bus LCD controller:

LCD_CS connected to ground or GPIO (normally to LOW should be ok to reduce timing)

LCD_RD connected to one FB_CSx

LCD_WR connected to one FB_CSx

LCD_RS connnected to GPIO or FB_ADx

LCD_D0..D15 conencted to FB_AD15 .. FB_AD31

Then you define two memory ranges for Wrtting or reading, the MCU will assert the corresponding CSx.

Luis

0 件の賞賛
返信
3,939件の閲覧回数
weblar
Contributor V

Hi Luis,

Thanks for your reply.

I shall stick with the 6800 mode then as that seems less complicated. I guess reading from the display is not really an issue given that I'm working with a frame buffer - I can just read the contents of that.

Best regards,

K

0 件の賞賛
返信