TWR-KM34_DEMO_SW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-KM34_DEMO_SW

1,553 Views
daido
Contributor II

Hi all,

Sample program _twr_emeter_demo displays wrong value.

1. Frequency

Displayed 24.870 Hz, applying 50.0 Hz.

2. kWh and kVArh

Increased about 2/3 of kWh value * seconds / 3600.

It seems auxcalc_callback() called @ 800Hz.

Give me any suggestions ?

0 Kudos
Reply
2 Replies

1,351 Views
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi,

I have moved your question to the community where you will get support on your issue.

If you have more questions related to this Freescale Product part then please post them in this community where This thread was moved.

Have a nice day.

Best Regards,

Garabo

0 Kudos
Reply

1,351 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, all,

sorry for the delay, as you know that there is K20 on the TWR-KM34Z50M, which generate 3 phase voltage and 3 phase current via PWM channels  to simulate the power system, the KM34 uses ADC to sample the 3 phase voltage and current signals and do the corresponding computation.

Unfortunately, I had tested the TWR-KM34Z50M board, but the Freemaster tools could not communicate.

sorry for not finding out the root cause.

BR

XiangJun Rong

0 Kudos
Reply