TWR-KM34_DEMO_SW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-KM34_DEMO_SW

1,543件の閲覧回数
daido
Contributor II

Hi all,

Sample program _twr_emeter_demo displays wrong value.

1. Frequency

Displayed 24.870 Hz, applying 50.0 Hz.

2. kWh and kVArh

Increased about 2/3 of kWh value * seconds / 3600.

It seems auxcalc_callback() called @ 800Hz.

Give me any suggestions ?

0 件の賞賛
返信
2 返答(返信)

1,341件の閲覧回数
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi,

I have moved your question to the community where you will get support on your issue.

If you have more questions related to this Freescale Product part then please post them in this community where This thread was moved.

Have a nice day.

Best Regards,

Garabo

0 件の賞賛
返信

1,341件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, all,

sorry for the delay, as you know that there is K20 on the TWR-KM34Z50M, which generate 3 phase voltage and 3 phase current via PWM channels  to simulate the power system, the KM34 uses ADC to sample the 3 phase voltage and current signals and do the corresponding computation.

Unfortunately, I had tested the TWR-KM34Z50M board, but the Freemaster tools could not communicate.

sorry for not finding out the root cause.

BR

XiangJun Rong

0 件の賞賛
返信