TWR-K70 + Usb Stack HID device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K70 + Usb Stack HID device

跳至解决方案
2,734 次查看
gaminn
Contributor IV

Hello,

I installed Freescale USB stack v4.0.2 and Codewarrior 10.3. I opened HID device sample project for K70 - Freescale USB Stack v4.0.2\Source\Device\app\hid\cw10\kinetis_k70 and downloaded it to my TWR-K70 via its integrated OSJTAG. Then connected second USB cable to micro connector of TWR-SER.

I get a message with yellow exclamation mark, that Win8 can't recognize USB device.

I get the same message when I run MSD sample project.

What's wrong???

标签 (2)
标记 (3)
1 解答
2,278 次查看
Pepe_Ruiz
Contributor IV

Hi Martin,

K70 has two different USB ports:

High-speed USB port can be accessed using TWR-SER2 board because you need the external USB HS PHY

Full-Speed USB port can be accessed using TWR-SER board

Are u opening the correct project for the USB module that you want?

also inside the documentation folder there is a file called USBHWCONFIG.pdf that shows the correct jumpers configuration for each board and use case.

Let me know if you still have problems and I will post more information.

regards

在原帖中查看解决方案

5 回复数
2,278 次查看
xavi2804
Contributor II

hello, im trying to use this USB stack HID device, but with the twr-ser2, i already define HS, but it doesnt do anything, also i checked the jumper, i have a question in my twr-k70F i cant find what does the J21 means?

0 项奖励
回复
2,278 次查看
Monica
Senior Contributor III

Martin,

was this helpful?

Please keep us posted!

Thanks!

0 项奖励
回复
2,278 次查看
gaminn
Contributor IV

Yes. Bad jumpers on TWR-SER.... Sorry not to post it here immediatelly and thanks for you advice.

2,278 次查看
Monica
Senior Contributor III

Great to know is now working!

Regards :smileyhappy:

0 项奖励
回复
2,279 次查看
Pepe_Ruiz
Contributor IV

Hi Martin,

K70 has two different USB ports:

High-speed USB port can be accessed using TWR-SER2 board because you need the external USB HS PHY

Full-Speed USB port can be accessed using TWR-SER board

Are u opening the correct project for the USB module that you want?

also inside the documentation folder there is a file called USBHWCONFIG.pdf that shows the correct jumpers configuration for each board and use case.

Let me know if you still have problems and I will post more information.

regards