TWR-K65F180M MQX BSP+DEMO APPLICATION

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR-K65F180M MQX BSP+DEMO APPLICATION

1,300 次查看
andrey_kartavi
Contributor I

Hello, I developed in the past K10 driver layer (BSP + driver library) that was based on MQX BSP of TWR-K20 EVB. My question is: I think to use K66 and to do the same but based on TWR-K65F180M. What SW tools should I use for it? Because now the tools are changed from CodeWarrior and MQX4.0.1. Is there some DEMO MQX project for it (like twrk20d72m.cw10gcc)? So I could adapt it for my hardware like I did for K10. Thanks. Andrey Kartavi. 

标签 (1)
0 项奖励
回复
2 回复数

1,292 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi @andrey_kartavi :

 

MQX v5 support K66.  It is under commercial license.   Please refer to below link for more details.

https://www.nxp.com/design/software/embedded-software/mqx-software-solutions/mqx-v5-software-solutio...

It also possible for you to port it by yourself.  The start point is the TWR-K65 BSP.

There is a port guider under the MQX installation folder

C:\Freescale\Freescale_MQX_4_2\doc\mqx

 

Regards

Daniel

 

0 项奖励
回复

1,286 次查看
andrey_kartavi
Contributor I

Thanks  Daniel Chen. I guess that MQX5 will have the same concept. MQX installation has the TWR-K65F180M project. And there is a tool to PORT to K66. 

0 项奖励
回复