TWR-K60N512 (Problems with first steps)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60N512 (Problems with first steps)

2,040 Views
admin
Specialist II

Hello!

 

I have bought TWR-K60N512. I also have installed:

1)IAR 5.50.6 

2)MQX 3.7 and kwickStik_Patch 

 

So I have problems at 4'th point of "Quick start":

 

I have found "build_libs.eww" and done everything with it. But when I had opened "TWR-K60N512_Quick_Start_Demo.eww" with IAR, it wrote:

 

1)The project 'TWR-K60N512_Quick_Start_Demo' contaains the unknown tool 'PEMICRO_ID' 

2)Invalid driver (/driver) option 

3) Invalid processor (/proc) option 

4)No kernel to load 

5)An error occured trying ti initialize the debugger. Debugging will not be available in this session 

 

What should I do?

 

0 Kudos
Reply
1 Reply

1,614 Views
anthony_huereca
NXP Employee
NXP Employee

You'll need to use IAR 6.10 or later. Earlier versions of IAR don't have support for OSJTAG, which is the built-in debugger on the tower boards.

 

You could alternatively use a JLink to program the board (which is supported in IAR 5.50), but you'd have to re-configure the project settings since opening the IAR 6.10 projects in IAR 5.50 corrupts the settings.

0 Kudos
Reply