After building MQX6.2 IAR IDE does not have the MQX tool bar tab as in the class.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After building MQX6.2 IAR IDE does not have the MQX tool bar tab as in the class.

2,386 Views
captmark
Contributor I

Hello,   

 

           In class with the K40 tower using my personnel lap top with a 30day eval from IAR I had no problem compiling and running all the labs. At work I can complie Lab 1 which does not use MQX rtos. If I try to run any lab using MQX I cannot compile the code.  Also I do not see the MQX tool bar tab that showed up with the 30 day eval.

              My IAR is ver 6.2 and when I batch build the MQX6.2 softwate I get no errors.

 

Can any one think of what could be wrong?

 

Thanks  Capt Mark

 

 

 

0 Kudos
Reply
3 Replies

2,179 Views
tr9
Contributor II

Hello Capt,

 

I am having a similar problem. Did you ever get an answer?

0 Kudos
Reply

2,179 Views
captmark
Contributor I

No I have not. I will be going to thr FTF in two weeks but hope to find answer before.

 

Capt

0 Kudos
Reply

2,179 Views
anthony_huereca
NXP Employee
NXP Employee

What kind of compile errors did you get? That can help narrow down what went wrong.

0 Kudos
Reply