TWR_K60_120MHz_SampleCode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR_K60_120MHz_SampleCode

跳至解决方案
3,106 次查看
priyagupta
Contributor II

The link attached for the sample code in below thread is not working, as it is 4 year old post.

https://community.nxp.com/thread/307951 

Can any one send me the link for the same(specially for USB & I2C)? It will be really very helpful for me.

Thanks !

标签 (1)
标记 (1)
1 解答
2,797 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Priya Gupta,

    I think the link in that post is changed, please download the sample code for TWR-K60F120M from this link :

Kinetis® 120MHz bare metal sample code

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
2,797 次查看
priyagupta
Contributor II

Thank you Kerry and Mark !! Really appreciate your help.

0 项奖励
回复
2,797 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Priya Gupta,

    You are welcome!

    If your question is solved, please mark the correct answer to close this question.

   Thank you and have a nice day!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,798 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Priya Gupta,

    I think the link in that post is changed, please download the sample code for TWR-K60F120M from this link :

Kinetis® 120MHz bare metal sample code

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,797 次查看
mjbcswitzerland
Specialist V

Hi Priya

The example code has moved through several generations of different solutions in the meantime so I doubt that the links will be supported in any way. I think that NXP will suggest you use SDK-2.2 instead, although I don't know whether the K60 is still supported.

You can however also get USB, I2C, TCP/IP etc. in the open source uTasker project at the links below (supports tower boards with TWR-SER or TWR-SER2 and FS and HS USB)

Regards

Mark

http://www.utasker.com/kinetis/TWR-K60N512.html
http://www.utasker.com/kinetis/TWR-K60D100M.html
http://www.utasker.com/kinetis/TWR-K60F120M.html

http://www.utasker.com/kinetis.html

USB:
- http://www.utasker.com/docs/uTasker/USB_User_Guide.PDF
- http://www.utasker.com/docs/uTasker/uTaskerV1.3_USB_Demo.PDF
- http://www.utasker.com/docs/uTasker/uTaskerUSB_Audio.pdf
- http://www.utasker.com/docs/uTasker/uTaskerRNDIS.pdf
- Composite http://www.utasker.com/kinetis/USB_Device.html

I2C
- http://www.utasker.com/docs/uTasker/uTasker_I2C.pdf

UART (interrupt and DMA diven)
- http://www.utasker.com/docs/uTasker/uTaskerUART.PDF

Ethernet Video - IPv4/IPv6 stack on K60 Tower kit
- https://www.youtube.com/watch?v=BMPXhtoUeJo&feature=youtu.be