TWR_K60_120MHz_SampleCode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR_K60_120MHz_SampleCode

ソリューションへジャンプ
3,221件の閲覧回数
priyagupta
Contributor II

The link attached for the sample code in below thread is not working, as it is 4 year old post.

https://community.nxp.com/thread/307951 

Can any one send me the link for the same(specially for USB & I2C)? It will be really very helpful for me.

Thanks !

ラベル(1)
タグ(1)
1 解決策
2,912件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Priya Gupta,

    I think the link in that post is changed, please download the sample code for TWR-K60F120M from this link :

Kinetis® 120MHz bare metal sample code

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,912件の閲覧回数
priyagupta
Contributor II

Thank you Kerry and Mark !! Really appreciate your help.

0 件の賞賛
返信
2,912件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Priya Gupta,

    You are welcome!

    If your question is solved, please mark the correct answer to close this question.

   Thank you and have a nice day!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,913件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Priya Gupta,

    I think the link in that post is changed, please download the sample code for TWR-K60F120M from this link :

Kinetis® 120MHz bare metal sample code

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,912件の閲覧回数
mjbcswitzerland
Specialist V

Hi Priya

The example code has moved through several generations of different solutions in the meantime so I doubt that the links will be supported in any way. I think that NXP will suggest you use SDK-2.2 instead, although I don't know whether the K60 is still supported.

You can however also get USB, I2C, TCP/IP etc. in the open source uTasker project at the links below (supports tower boards with TWR-SER or TWR-SER2 and FS and HS USB)

Regards

Mark

http://www.utasker.com/kinetis/TWR-K60N512.html
http://www.utasker.com/kinetis/TWR-K60D100M.html
http://www.utasker.com/kinetis/TWR-K60F120M.html

http://www.utasker.com/kinetis.html

USB:
- http://www.utasker.com/docs/uTasker/USB_User_Guide.PDF
- http://www.utasker.com/docs/uTasker/uTaskerV1.3_USB_Demo.PDF
- http://www.utasker.com/docs/uTasker/uTaskerUSB_Audio.pdf
- http://www.utasker.com/docs/uTasker/uTaskerRNDIS.pdf
- Composite http://www.utasker.com/kinetis/USB_Device.html

I2C
- http://www.utasker.com/docs/uTasker/uTasker_I2C.pdf

UART (interrupt and DMA diven)
- http://www.utasker.com/docs/uTasker/uTaskerUART.PDF

Ethernet Video - IPv4/IPv6 stack on K60 Tower kit
- https://www.youtube.com/watch?v=BMPXhtoUeJo&feature=youtu.be