TRGMUX Port Pin Trigger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TRGMUX Port Pin Trigger

ソリューションへジャンプ
2,398件の閲覧回数
jh0
Contributor IV

Hi,

I want to start/stop FlexIO timers with one (non FlexIO) port pin. When pin goes high, timers are started, and when pin goes low, timers are stopped.

I configured (port A pin 1) with PORT PCR values MUX 1 (GPIO) and IRQC 13 (Enable active high trigger output, flag is disabled. [The trigger output goes to the trigger mux, which allows pins to trigger other peripherals (configurable polarity; 1 pin per port; if multiple pins are configured, then they are ORed together to create the trigger)].

I configured TRGMUX_FLEXIO0 with SEL0 value 0x2A Port A Pin Trigger is selected.

Also configured FlexOI timers and everything is working fine, as expected.

But when I change state of other pin on port A, this have influence on trigger, and I don't understand why, because for all other pins on the same port A, IRQC value in PCR is zero. How I can isolate trigger to just one port pin?

Device is K32L2A31.

Regards,

Josip

タグ(1)
0 件の賞賛
返信
1 解決策
2,365件の閲覧回数
jh0
Contributor IV

Hi Felipe,

I just made simple program with few lines of code to demonstrate this, together with scope screenshots, to attach all together here.

But, everything is working fine as it should. Only port pin that is triggering FlexIO timers start / stop is one pin with  IRQC 13. Other pins with IRQC 0 doesn't disturb FlexIO timers on any way. So everything is OK with device, problem is somewhere else in my code.

Regards,

Josip

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,366件の閲覧回数
jh0
Contributor IV

Hi Felipe,

I just made simple program with few lines of code to demonstrate this, together with scope screenshots, to attach all together here.

But, everything is working fine as it should. Only port pin that is triggering FlexIO timers start / stop is one pin with  IRQC 13. Other pins with IRQC 0 doesn't disturb FlexIO timers on any way. So everything is OK with device, problem is somewhere else in my code.

Regards,

Josip

0 件の賞賛
返信
2,376件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Josip,

Could you please share the code you are using to configure TRGMUX? I would like to investigate this in more detail.

Best regards,

Felipe

0 件の賞賛
返信