System hangs with simultaneous QSPI file access and XiP execution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

System hangs with simultaneous QSPI file access and XiP execution

ソリューションへジャンプ
3,243件の閲覧回数
deniscollis
Contributor V

I have a K8x with a single-die 16MB QSPI flash module.  The QSPI memory layout is arranged with a section for XiP code, and another section for a file system.  If a function in internal flash accesses the file system, then everything works fine. Functions on external flash that do not access the file system also run without a problem.  However, if a function on QSPI flash attempts to access the file system, also on QSPI flash, then the system hangs.  In the debugger I see that the QSPI busy bit (BOARD_QSPI_BASE->SR & QuadSPI_SR_BUSY_MASK) remains set, forever.

How can this be overcome?

ラベル(1)
タグ(5)
1 解決策
3,037件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Denis,

 

Unfortunately, what you are trying to do is not possible. Accessing the file system at the same time the code is running from the QSPI memory it is a limitation of XiP.

 

For implementing this you will have to execute the function from internal flash or either copy the function to ram and execute it from there.

 

Best regards,

Felipe

元の投稿で解決策を見る

2 返答(返信)
3,038件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Denis,

 

Unfortunately, what you are trying to do is not possible. Accessing the file system at the same time the code is running from the QSPI memory it is a limitation of XiP.

 

For implementing this you will have to execute the function from internal flash or either copy the function to ram and execute it from there.

 

Best regards,

Felipe

3,037件の閲覧回数
deniscollis
Contributor V

Hi Felipe,

I found a similar discussion - RT1050 QSPI Flash Limitations - which confirms your answer.  I'm assuming that memory-mapped reads from the file-system will be okay, and it's just the functions that control erase- and write-cycles that must be located in RAM or internal flash.

Thanks,

Denis