Stock firmware for the TWR-K21D50M

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Stock firmware for the TWR-K21D50M

跳至解决方案
1,823 次查看
jorgesierra
Contributor II

Where do I find the firmware that comes with this board? I'm asking for the S19 or srec or anything of the like so I can undo any of the changes when I start using the cyclone max.

0 项奖励
回复
1 解答
1,743 次查看
adriancano
NXP Employee
NXP Employee

Hi Jorge,

You can get from here TWR-K21D50M Sample Code the sample code for the board, inside the folder that is installed in the next path TWR-K21D50M Sample Code\TWR-K21D50M_SC\build\cw\TWR-K21D50M-OOBE you can find the Out of the Box demo for the board, this is the source code for the demo, you can find the version for IAR IDE also.

I hope this information can help you.

Regards,

Adrian

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,744 次查看
adriancano
NXP Employee
NXP Employee

Hi Jorge,

You can get from here TWR-K21D50M Sample Code the sample code for the board, inside the folder that is installed in the next path TWR-K21D50M Sample Code\TWR-K21D50M_SC\build\cw\TWR-K21D50M-OOBE you can find the Out of the Box demo for the board, this is the source code for the demo, you can find the version for IAR IDE also.

I hope this information can help you.

Regards,

Adrian

0 项奖励
回复
1,743 次查看
jorgesierra
Contributor II

Thanks. In the future, where would I have found this if I didn't have this forum to save my life?

0 项奖励
回复