Stock firmware for the TWR-K21D50M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stock firmware for the TWR-K21D50M

ソリューションへジャンプ
1,846件の閲覧回数
jorgesierra
Contributor II

Where do I find the firmware that comes with this board? I'm asking for the S19 or srec or anything of the like so I can undo any of the changes when I start using the cyclone max.

0 件の賞賛
返信
1 解決策
1,766件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi Jorge,

You can get from here TWR-K21D50M Sample Code the sample code for the board, inside the folder that is installed in the next path TWR-K21D50M Sample Code\TWR-K21D50M_SC\build\cw\TWR-K21D50M-OOBE you can find the Out of the Box demo for the board, this is the source code for the demo, you can find the version for IAR IDE also.

I hope this information can help you.

Regards,

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,767件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi Jorge,

You can get from here TWR-K21D50M Sample Code the sample code for the board, inside the folder that is installed in the next path TWR-K21D50M Sample Code\TWR-K21D50M_SC\build\cw\TWR-K21D50M-OOBE you can find the Out of the Box demo for the board, this is the source code for the demo, you can find the version for IAR IDE also.

I hope this information can help you.

Regards,

Adrian

0 件の賞賛
返信
1,766件の閲覧回数
jorgesierra
Contributor II

Thanks. In the future, where would I have found this if I didn't have this forum to save my life?

0 件の賞賛
返信