Stock firmware for the TWR-K21D50M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stock firmware for the TWR-K21D50M

Jump to solution
1,853 Views
jorgesierra
Contributor II

Where do I find the firmware that comes with this board? I'm asking for the S19 or srec or anything of the like so I can undo any of the changes when I start using the cyclone max.

0 Kudos
Reply
1 Solution
1,773 Views
adriancano
NXP Employee
NXP Employee

Hi Jorge,

You can get from here TWR-K21D50M Sample Code the sample code for the board, inside the folder that is installed in the next path TWR-K21D50M Sample Code\TWR-K21D50M_SC\build\cw\TWR-K21D50M-OOBE you can find the Out of the Box demo for the board, this is the source code for the demo, you can find the version for IAR IDE also.

I hope this information can help you.

Regards,

Adrian

View solution in original post

0 Kudos
Reply
2 Replies
1,774 Views
adriancano
NXP Employee
NXP Employee

Hi Jorge,

You can get from here TWR-K21D50M Sample Code the sample code for the board, inside the folder that is installed in the next path TWR-K21D50M Sample Code\TWR-K21D50M_SC\build\cw\TWR-K21D50M-OOBE you can find the Out of the Box demo for the board, this is the source code for the demo, you can find the version for IAR IDE also.

I hope this information can help you.

Regards,

Adrian

0 Kudos
Reply
1,773 Views
jorgesierra
Contributor II

Thanks. In the future, where would I have found this if I didn't have this forum to save my life?

0 Kudos
Reply