Stacking FRDM K64F and OM5578 and SE050ARD arduino shields

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stacking FRDM K64F and OM5578 and SE050ARD arduino shields

ソリューションへジャンプ
3,662件の閲覧回数
douglas_tan
Contributor I

I'm a newcomer to embedded electronics and have read some introductions about SPI/I2C/UART on sparkfun.

I'll like to know whether the OM5578 (PN7150) and SE050ARD Arduino shields can be stacked together on a Freedom K64F devboard. 

I tried looking at the schematics in AN12395 and UM10935 and it looks like I2C is used by both the OM5578 and SE050ARD via the Arduino header to the K64F. I2C is supposed to manage multiple slaves (OM5578 / SE050ARD) connected to the master (K64F) so would there be any bus contention issues here? Also would it be safe (i.e avoid damaging the devboards) to stack the 3 boards together?

I found  https://community.nxp.com/docs/DOC-344305 which does something similar. Would this be applicable to my scenario here?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,487件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Douglas,

I received confirmation on the following:

1. Make sure that both shields are configured as slaves and the master is K64. 

2. The SE050 has an NFC tag, please keep this in mind when using the PN7150 since if it is enabled it will always be reading that tag.

Other than that there should not be a problem

Best Regards,

Sabina

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,487件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Douglas,

Hope you are doing well.

I am confirming this information for you. However, from a first look it doesn't look like there should be any problem connecting the three as it should not demand much current consumption. I'd like to ask you if you were able to get the SE050ARD working with the K64 board on their own? 

I believe it will be the jumper configuration on the SE050RD board that will allow further I2C communication with the PN7150. I will update you on this once I get confirmation if this is correct.

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信
3,487件の閲覧回数
douglas_tan
Contributor I

Hey Sabina,

I can confirm that the SE050ARD works with the K64 board on its own. Thanks for your help.

0 件の賞賛
返信
3,488件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Douglas,

I received confirmation on the following:

1. Make sure that both shields are configured as slaves and the master is K64. 

2. The SE050 has an NFC tag, please keep this in mind when using the PN7150 since if it is enabled it will always be reading that tag.

Other than that there should not be a problem

Best Regards,

Sabina

0 件の賞賛
返信
3,239件の閲覧回数
BANGYUD
Contributor II

halo, i got error when intergrated pn7150 with arduino , can you help me, i can't read the tag type B 

0 件の賞賛
返信
3,487件の閲覧回数
douglas_tan
Contributor I

Thanks for looking into this Sabina. I resorted to connecting the 3 boards onto a breadboard to test and verified that there's no issue with i2c connectivity in this setup.

0 件の賞賛
返信
3,487件の閲覧回数
douglas_tan
Contributor I

Looking up the docs, it looks like the OM5578 and SE050 use different I2C addresses. So I stacked them together with the OM5578 on top of the SE050. 

However, there's apparently an issue with this as I'm unable to run the NXPNCI example for K64F

Running the NXP-NCI project.
Error: cannot connect to NXPNCI device

This same example runs as expected when the OM5578 is connected to the K64F directly. Is there anywhere I should start looking?

0 件の賞賛
返信