Source of LLWU wakeup from VLLS3 on K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source of LLWU wakeup from VLLS3 on K60

Jump to solution
1,487 Views
Karts
Contributor I

Hello,

Please find the attached for screenshot.Apparently,the WAKEUP bit in "Mode Control" register is set to 1.However,i do not know which module caused that reset.I have associated couple of timers and a couple of IO pins to LLWU module to wake up K60 chip from VLLS3 mode.

Is there a register to know which peripheral or IO pin triggered LLWU module to reset the K60(which i assume is waking up K60 from VLLS3 mode)?

Thanks.

Regards,

Karthik

Labels (1)
0 Kudos
Reply
1 Solution
1,282 Views
apanecatl
Senior Contributor II

To know which  wake up source caused the reset you need to check registers LLWU_F1, LLWU_F2 and LLWU_F3

View solution in original post

0 Kudos
Reply
1 Reply
1,283 Views
apanecatl
Senior Contributor II

To know which  wake up source caused the reset you need to check registers LLWU_F1, LLWU_F2 and LLWU_F3

0 Kudos
Reply