Software Used to download Firmware image to K60.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Software Used to download Firmware image to K60.

跳至解决方案
1,465 次查看
danielchai
Senior Contributor I

Hi All,

I generate a binary image file for my application.

I am wondering if there is a software that I can use to update the application image on the K60N512 board?

Thanks.

-Daniel

标记 (3)
0 项奖励
回复
1 解答
1,299 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Daniel,

I think you may use IAR, CodeWarrior or Keil to download the bin image, if you only need a tool to program the device, you may use the EzPort interface, which is a SPI like interface, and we provide an app note on that topic, please kindly refer to http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4406.pdf?fsrch=1&sr=1 for more details.

Hope that helps,

B.R

Kan

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,300 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Daniel,

I think you may use IAR, CodeWarrior or Keil to download the bin image, if you only need a tool to program the device, you may use the EzPort interface, which is a SPI like interface, and we provide an app note on that topic, please kindly refer to http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4406.pdf?fsrch=1&sr=1 for more details.

Hope that helps,

B.R

Kan

0 项奖励
回复
1,299 次查看
danielchai
Senior Contributor I

Hi Kan,

It is exactly what I need.

Thank you.

0 项奖励
回复