Software Used to download Firmware image to K60.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software Used to download Firmware image to K60.

Jump to solution
1,463 Views
danielchai
Senior Contributor I

Hi All,

I generate a binary image file for my application.

I am wondering if there is a software that I can use to update the application image on the K60N512 board?

Thanks.

-Daniel

Tags (3)
0 Kudos
Reply
1 Solution
1,297 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Daniel,

I think you may use IAR, CodeWarrior or Keil to download the bin image, if you only need a tool to program the device, you may use the EzPort interface, which is a SPI like interface, and we provide an app note on that topic, please kindly refer to http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4406.pdf?fsrch=1&sr=1 for more details.

Hope that helps,

B.R

Kan

View solution in original post

0 Kudos
Reply
2 Replies
1,298 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Daniel,

I think you may use IAR, CodeWarrior or Keil to download the bin image, if you only need a tool to program the device, you may use the EzPort interface, which is a SPI like interface, and we provide an app note on that topic, please kindly refer to http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4406.pdf?fsrch=1&sr=1 for more details.

Hope that helps,

B.R

Kan

0 Kudos
Reply
1,297 Views
danielchai
Senior Contributor I

Hi Kan,

It is exactly what I need.

Thank you.

0 Kudos
Reply