Smallest Kinetis uC with CAN?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Smallest Kinetis uC with CAN?

2,347 Views
christhomas
Contributor II

Hi, I am looking for an ARM microcontroller with the smallest footprint that contains CAN. Is there possibly a WLCSP package for it? Thanks in advance.

3 Replies

2,261 Views
mjbcswitzerland
Specialist V

Hi Chris

There are a few in WLCSP with CAN: Kinetis® Mini MCUs: Wafer-Level Chip-scale Packages (WLCSP) based on Arm® Cortex®-M0+/M4 Core|NXP 

such as K20 and K60.

Regards

Mark

0 Kudos
Reply

2,261 Views
christhomas
Contributor II

Hi Mark,

Thanks for that. I guess the smallest Kinetis processor with a CAN transceiver would be 5mm x 5mm. Am I correct?

0 Kudos
Reply

2,261 Views
mjbcswitzerland
Specialist V

 Chris

K20 or K60 ones in 5.3x 5.3 x 0.6mm
or
K24 one in 4.8 x 5.6 x 0.6mm

Regards

Mark