Documentation of SRS and SSRS Registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Documentation of SRS and SSRS Registers

1,050 Views
Keith4DSmith
Contributor V

In document K22P121M120SF7RM Rev 4 8/2016 is documentation for both SRS and SSRS registers in Reset Control, RCM, Chapter 13

In document K22P144M120SF5V2RM Rev. 5 March 2015 is documentation of the SRS registers in Reset Control Module, RCM, Chapter 14.

Does this mean that some K22s do not support SSRS registers or is this missing documentation?

Labels (1)
0 Kudos
Reply
1 Reply

961 Views
mjbcswitzerland
Specialist V

Hi Keith

F5 and F7 (K22) devices are not the same - check carefully which of the documents is relevant for the exact part that you use.

If you compare carefully there are a number of differences (often SW incompatible) between the various K22 devices.

For example F7 parts (ones with 128k or 512k Flash without NVRAM) have different base addresses for ADC1, have an additional options register (SIM_OPT8), have some different peripheral clocking controls (SIM_SCGC1). Also they have HSRUN mode to operate above 80MHz, whereas the F5 parts can run at 120MHz without the HSRUN mode restrictions. Some parts use long word Flash programming and others use phrase programming (so need different Flash drivers).......

There are more and I think that there is a document somewhere listing all of the things that need to be taken into account.

Regards

Mark

0 Kudos
Reply