Simultaneous High speed USB transfer with eDMA transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simultaneous High speed USB transfer with eDMA transfer

ソリューションへジャンプ
2,336件の閲覧回数
mrharmonsr
Contributor III

Using a K64 MCU - MK61FN1M0VMJ12

I want to transfer data into memory from an external peripheral AND transfer data from memory via high speed USB at the same time.  Currently I am doing these operations sequentially.

I can't find information about the relative priority of the two BUS masters, is it documented?

I assume the two transfers will share the bus, only using the cycles needed.

Can anyone point me to some documentation on the topic?

Larry

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,199件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Larry,

The K64 reference manual chapter 3.3.6 shows the crossbar switch configuration.

The ARM core as Master0, DMA as Master2 and USB module as Master4 using crossbar to access slave device.

pastedImage_1.png

The K64 reference manual chapter18 shows how to set crossbar switch for master with different priority to access slave.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,199件の閲覧回数
mrharmonsr
Contributor III

I finally have a working solution.  Initially I used SRAM to hold buffers and HSUSB descriptors.  This works well, but consumes a lot of SRAM.

I was able to get everything working in DDR by a combination of using the aliased DDR address space for USB descriptors and buffers and changing the crossbar priorities for the DDR (Slave 5) with HSUSB at the highest priority followed by eDMA then the ARM Core.

0 件の賞賛
返信
2,200件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Larry,

The K64 reference manual chapter 3.3.6 shows the crossbar switch configuration.

The ARM core as Master0, DMA as Master2 and USB module as Master4 using crossbar to access slave device.

pastedImage_1.png

The K64 reference manual chapter18 shows how to set crossbar switch for master with different priority to access slave.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信