Silicon rev difference in K22 series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Silicon rev difference in K22 series

1,759 次查看
gandhamb
Contributor I

Can you help in Difference between parts  MK22FN1M0VLQ12 & MK22FN1M0AVLQ12.

As per our comparison,we could find that the difference is only silicon revision  i.e blank for main and A for after main revision from datasheet.other all functions ,pin defenition s, footprint, thermal characterics, reliability  etc remains same.is our understanding correct?

currently we had struck in the design because of components non availability in market.

MK22FN1M0VLQ12 part is available from some suppliers but it is not recommended for new designs as per Nxp website and still in longivety program.

MK22FN1M0AVLQ12 is the part we planned for design but not available in the market.

so we are planning to use MK22FN1M0VLQ12 for proto development and then when the actual MK22FN1M0AVLQ12 is available will replace with that.

Will this  approach works or not?please comment 

0 项奖励
回复
1 回复

1,741 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi gandhamb,

We have a community document giving a general look at the changes between the different versions which can be found here. This document also includes a link to the Engineering Bulletin with additional information. Still, for specific changes between revisions, we recommend checking the Errata Mask documents available here.

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复