Set the system clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set the system clock

Jump to solution
1,769 Views
李志權
Contributor II

I think the time is set to the following results:

The kernel/system clock          96MHz

The bus  clock                        48MHz

The Flex Bus clock                 48MHz

Flash clock                            24MHz

How to set up?

Best can have pictures of codewarrior operation

I am using is TWR - K60D100M development board

Labels (1)
0 Kudos
Reply
1 Solution
1,524 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I think you can refer it:

clock.jpg

Hope that help

View solution in original post

0 Kudos
Reply
1 Reply
1,525 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I think you can refer it:

clock.jpg

Hope that help

0 Kudos
Reply