Set the system clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,854件の閲覧回数
李志權
Contributor II

I think the time is set to the following results:

The kernel/system clock          96MHz

The bus  clock                        48MHz

The Flex Bus clock                 48MHz

Flash clock                            24MHz

How to set up?

Best can have pictures of codewarrior operation

I am using is TWR - K60D100M development board

ラベル(1)
0 件の賞賛
返信
1 解決策
1,609件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I think you can refer it:

clock.jpg

Hope that help

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,609件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I think you can refer it:

clock.jpg

Hope that help

0 件の賞賛
返信