Set EEPROM size code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,371件の閲覧回数
hayouniaymen
Contributor I

Hi,

I'm using the driver example of flexnvm_eeprom in SDk2.

and I need to change the size code of the EEPROM from 32bytes (mentioned in the demo : #define EEPROM_DATA_SET_SIZE_CODE (0x39U) )  to 3K.

How can I poursuit to change the size please?

0 件の賞賛
返信
1 解決策
2,267件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hayouni,

  Please tell me what the kinetis chip you are using? Please tell me the chip part number.

  I will help you to check it.

Actually, you can check that chip's reference manual, flash chapter, to check the partition content.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,268件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hayouni,

  Please tell me what the kinetis chip you are using? Please tell me the chip part number.

  I will help you to check it.

Actually, you can check that chip's reference manual, flash chapter, to check the partition content.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,267件の閲覧回数
hayouniaymen
Contributor I

Thank's Kerry,

I checked the reference manual and i m able now to change the data size code of the EEPROM partition.

0 件の賞賛
返信