I'm attempting to program a K81 and QSPI (Micron MT25QL128 - 16MB, single die). Segger J-Flash V7.54c shows error:
Timeout while preparing target, RAMCode did not respond in time. (PC = 0x00000000, CPSR = 0x00000000, LR = 0x61000000)!
Failed to prepare RAMCode using RAM
Error while determining flash info (Bank 1 @ 0x68000000)
Failed to auto program target
The J-Flash Project Info:
Has anyone encountered this, and can figure what's going on?
Thanks,
Denis
解決済! 解決策の投稿を見る。
J-Flash/J-Link V6.50a works perfectly. There's a bug in V7.45c, which I have reported to Segger.
Update Jan 20, 2022 from Segger:
Upcoming release of Segger J-Link/J-Flash will include fix for this issue.
The issue was due to a speed optimization that relied on the availability of an external reference clock, RTCK, which is not the case with many devices, including the NXP K8x.
Update Jan 25, 2022:
Segger J-Link/J-Flash V7.60f available for download. Fix for K8x issue included in this release.
J-Flash/J-Link V6.50a works perfectly. There's a bug in V7.45c, which I have reported to Segger.
Update Jan 20, 2022 from Segger:
Upcoming release of Segger J-Link/J-Flash will include fix for this issue.
The issue was due to a speed optimization that relied on the availability of an external reference clock, RTCK, which is not the case with many devices, including the NXP K8x.
Update Jan 25, 2022:
Segger J-Link/J-Flash V7.60f available for download. Fix for K8x issue included in this release.
Hi,
When you use jFlash, you doesn't configure the QSPI. So the external ram can't be used.
Have a great day,
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
@nxf56274I'm not sure what you're saying. There is no external RAM, only the K81 with its onboard internal RAM.
As I understand the process, in order to write to the external QSPI flash, j-Flash/J-Link first downloads code to the MCU's internal RAM, sets the program counter and starts execution. Thereafter, J-Link/J-Flash sends instructions and data to the RAM resident code, which relays it to the external QSPI flash.
Thanks,
Denis