Secure Authentication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure Authentication

ソリューションへジャンプ
2,520件の閲覧回数
nidhintomy
Contributor IV

  

What is the scope of "SCOP3 and SESSION" in SE050 Examples?

Do we use it for IoT applications ?

0 件の賞賛
返信
1 解決策
2,499件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Yes, they are normally used in IoT applications. Please kindly refer to "3.7 Sessions " in https://www.nxp.com/webapp/Download?colCode=AN12543 and https://globalplatform.org/wp-content/uploads/2014/07/GPC_2.2_D_SCP03_v1.1.1.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,500件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Yes, they are normally used in IoT applications. Please kindly refer to "3.7 Sessions " in https://www.nxp.com/webapp/Download?colCode=AN12543 and https://globalplatform.org/wp-content/uploads/2014/07/GPC_2.2_D_SCP03_v1.1.1.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------