Secure Authentication

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Secure Authentication

跳至解决方案
2,524 次查看
nidhintomy
Contributor IV

  

What is the scope of "SCOP3 and SESSION" in SE050 Examples?

Do we use it for IoT applications ?

0 项奖励
回复
1 解答
2,503 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Yes, they are normally used in IoT applications. Please kindly refer to "3.7 Sessions " in https://www.nxp.com/webapp/Download?colCode=AN12543 and https://globalplatform.org/wp-content/uploads/2014/07/GPC_2.2_D_SCP03_v1.1.1.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,504 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Yes, they are normally used in IoT applications. Please kindly refer to "3.7 Sessions " in https://www.nxp.com/webapp/Download?colCode=AN12543 and https://globalplatform.org/wp-content/uploads/2014/07/GPC_2.2_D_SCP03_v1.1.1.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------