Sanity Check (K22FX512A)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sanity Check (K22FX512A)

4,814 Views
lsrbigfoot
Contributor IV

Is MK22FX512VLQ12 (Mask Set 1N41K) the exact same P/N as MK22FX512AVLQ12?

Also is MK22FX512VMD12 (Mask Set 1N41K) the exact same P/N as MK22FX512AVMD12?

 

I ask this because the MCU parts I've been using have the 'K22FX512' (1N41K) markings when I expected to see 'K22FX512A' (1N41K).

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

4,715 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi lsrbigfoot ,

Thank you for your interest in NXP kinetis product, I would like to provide service for you.
 talk the difference between MK22FX512VLQ12 and MK22FX512AVLQ12
MK22FX512AVLQ12 is nearly the same as MK22FX512VLQ12 .
But MK22FX512AVLQ12 have more uart register than MK22FX512VLQ12 , it is:
ARTX_AP7816A_T0, UARTX_AP7816B_T0,UARTX_WP7816A_T0,UARTX_WP7816A_T1,UARTX_WP7816B_T0,UARTX_WP7816B_T1,UARTX_WG7816_T1,UARTX_WP7816C_T1,

 Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------


.

0 Kudos
Reply

4,712 Views
lsrbigfoot
Contributor IV

I remember that some documentation was posted in the past which I found to be a little confusing:

https://www.nxp.com/docs/en/engineering-bulletin/EB811.pdf 

Kinetis K22_120 MHz devices 

EB811 mentioned MK22FX512A under Mask Set 1N41K but MK22FX512 under a different mask (3N03G).

So I have attached pics of the 2 MCU parts in question. The mask set on both parts is 1N41K but are marked as MK22FX512VLQ12/VMD12

Are these parts indeed MK22FX512VLQ12/VMD12 and not MK22FX512AVLQ12/VMD12?

Thanks in advance for the clarification.

0 Kudos
Reply

4,712 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi lsrbigfoot

  You attached picture chip is not MK22FX512AVLQ12/VMD12, it is  MK22FX512VLQ12/VMD12.

  If it is "A", the chip partnumber in the chip will contains "A".

  So, you don't need to consider  MK22FX512AVLQ12/VMD12, still use MK22FX512VLQ12/VMD12.

 Wish it helps you!

If you still have questions about it, please kindly let me know.

 

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply