Anybody used the example code from the FRDM-K66F "freedom bootloader" to run the bootloader MCUBOOT on a own design K66F board?
I've tried the example "freedom bootloader" on my FRDM-K66F board with getting a connection via USB terminal and blhost software. Seems to work fine until I flash the example "led_demo_freedom_a000". After writing this application into the µC, the bootloader can not be reached anymore. Boot switch does not help.
If I try to port the bootloader to my own PCB with TQFP version - yes, i've changed the package in the project, boot pin as well - i get no access to the bootloader. Same USB1 as the frdm-k66f board and for other usb examples my board works perfectly fine.
Any idea???
Hardware
PC: Win10 or Ubuntu 18.04
Board: FRDM-K66F (K20 processor bricked - programming via SEGGER JLINK Plus on J9)
Own Board: LQFP version K66F MK66FN2M0VLQ18 - USB1 used for Bootloader - reference design of FRDM-K66F used
MCUXpresso 11.1.1
SDK 2.7