SREC AND S19 files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SREC AND S19 files

7,330件の閲覧回数
pasini
Contributor I

Are srec and s19 the same files ? Is it just a different extension ?

How can I convert srec generated by IAR compiler ( K60N512 MCU ) to s19 ?

Thanks

Luiz

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

5,675件の閲覧回数
mjbcswitzerland
Specialist V

Luiz

Yes, s19 and SREC are the same. They are just two commonly used file name extensions for the same format.

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

5,675件の閲覧回数
jashanm
Contributor III

Hi Luiz,

         1   In CW software 'right click on the project' to choose 'properties'

         2   choose 'Settings' under 'C/C++ Build'

         3   Under 'Tool Settings' choose 'Additional Tools' and check 'Create Flash Image'

         4   Click 'Ok'

         5   Build the project now

         6   Follow steps 1 and 2 again

         7   Under 'Tool Settings' under 'ARM Ltd Windows GNU Create Flash Image' click 'Output'

         8   Select 'srec' under Output file format drop down menu

         9   Click 'Ok'

        10  Build the Project again

        11  Now you can find an '.hex' file under 'FLASH' folder

        12  Change the format to '.s19' to use it further

this is how you generate '.s19' file...

Regards,

Jashan

0 件の賞賛
返信