SPIMaster_Ldd Slave select Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPIMaster_Ldd Slave select Issue

Jump to solution
5,742 Views
kigerzhang
Contributor I

In a project based on KEAZ128 , the PE  component  "SPIMaster_Ldd"  was used . 

The  slave select signals were configured as GPIO . But the CS output is wrong  as shown in the following picture:

SPI CLOCK=500KHz

keaz128_spi0_SPIMaster_LDD.JPG

The IDE: 

- CodeWarrior for MCU
Version: 10.7
Build Id:160721

 The spi write code :

#define SPI0_SLAVE_CS_CTRL (UI_PTE->PDOR)

#define SPI0_SLAVE_CS_ALL 0x00000038
#define SPI0_SLAVE_CS_MASK 0x00000008

void spi0_write(uint8_t spi_slave_id,uint8_t data)
{
    SPI0_SLAVE_CS_CTRL |= SPI0_SLAVE_CS_ALL; // all cs bit set to 1

    SPI0_SLAVE_CS_CTRL &= ~(SPI0_SLAVE_CS_MASK << spi_slave_id); //active the slave

    (void)SM1_SendBlock(SM1_DeviceData, &data, sizeof(data));
    while(! SM1_GetBlockSentStatus(SM1_DeviceData)){}

    SPI0_SLAVE_CS_CTRL |= SPI0_SLAVE_CS_ALL; // all cs bit set to 1
}

Why the CS single   goes HIGH before the clock?

**************************************************************************************************************

I tried different setting:

SPI CLOCK=250KHz

keaz128_spi0_SPIMaster_LDD_250KHz.JPG

SPI CLOCK=1MHz

keaz128_spi0_SPIMaster_LDD_1MHz.JPG

SO,  the function "SM1_GetBlockSentStatus"  DO NOT work!    A bug? 

 

Need dig into the SPIMaster_Ldd code to check how the function to work. 

0 Kudos
Reply
1 Solution
5,315 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The key point in that document is to check the SPRF flag.

The Solution.png

SPI_send.png
Only this flat is able to indicate the shift register is received in(sent out) done.

SPI0_S[SPRF].png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
5,315 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kiger Zhang,

Sorry for my late reply!

Please refer the answer in Trouble using SPI GetBlockSentStatus():

It actually set the SerFlag when you push all the bytes in the TxFIFO and it doesn´t wait for the data to be shifted

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
5,315 Views
kigerzhang
Contributor I

Dear Robin,

Thanks for your reply. 

But I check the datasheet and the SPI PDD code ,it seems that the  SPI module in KEAZ128 device  does NOT have a "EOQ" bit.   So the solution for K64 does not work for Keaz128.

Any more suggestion?

0 Kudos
Reply
5,315 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes. The SPI module of KEAZ128 does NOT have a "EOQ" bit.
Due to lack of EOQ flag, you may need to refer the Solution described in L-Series SPI GPIO CS/SS.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
5,315 Views
kigerzhang
Contributor I

Dear Robin,

Thank you so much for your support. 

I checked the document  (  L-Series SPI GPIO CS/SS.) that you pointed to . 

The key point in that document is to check the  SPTEF  flag . 

I  digged into the function "SM1_GetBlockSentStatus"  of  SPIMaster_Ldd ,it does  the same thing. 

***************************************

In file SPI_PDD.h 

...

#define SPI_PDD_TX_BUFFER_EMPTYG SPI_S_SPTEF_MASK /**< Transmit buffer or FIFO empty flag. */

...

In file SM1.C 

 uint8_t StatReg = SPI_PDD_ReadStatusReg(SPI0_BASE_PTR); /* Read status register */

...

if ((StatReg & SPI_PDD_TX_BUFFER_EMPTYG) != 0U) { /* Is HW Tx buffer empty? */
if (DeviceDataPrv->OutSentDataNum < DeviceDataPrv->OutDataNumReq) { /* Is number of sent characters less than the number of requested incoming characters? */
SPI_PDD_WriteData8Bit(SPI0_BASE_PTR, (*((uint8_t *)DeviceDataPrv->OutDataPtr++))); /* Put a character with command to the transmit register and increment pointer to the transmitt buffer */
DeviceDataPrv->OutSentDataNum++; /* Increment the counter of sent characters. */
if (DeviceDataPrv->OutSentDataNum == DeviceDataPrv->OutDataNumReq) {
DeviceDataPrv->OutDataNumReq = 0x00U; /* Clear the counter of characters to be send by SendBlock() */
DeviceDataPrv->SerFlag |= BLOCK_SENT; /* Set data block sent flag */
SM1_OnBlockSent(DeviceDataPrv->UserData);
}
} else {
SPI_PDD_DisableInterruptMask(SPI0_BASE_PTR, SPI_PDD_TX_BUFFER_EMPTY); /* Disable TX interrupt */
}
}

********************************************

In fact the root cause is : the data in the TX buffer is moved to shift register so fast , but the data in the shift register should be sent out to the pin based on the  SCK .   

In page 534 of KEA128RM , the STPEF  description:

" ...

SPTEF is automatically set when all data from the transmit buffer transfers into the transmit shift register. For an idle  SPI, data written to D is transferred to the shifter almost immediately so that SPTEF is set within two bus cycles, allowing a second set of data to be queued into the transmit buffer. After completion of the transfer
of the data in the shift register, the queued data from the transmit buffer automatically moves to the shifter,
and SPTEF is set to indicate that room exists for new data in the transmit buffer. ..."

So ,what I want to know is : whether is there a flat to indicate that the shift register is sent out done, at that time the CS pin can be toggled.

0 Kudos
Reply
5,316 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The key point in that document is to check the SPRF flag.

The Solution.png

SPI_send.png
Only this flat is able to indicate the shift register is received in(sent out) done.

SPI0_S[SPRF].png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
5,315 Views
kigerzhang
Contributor I

Dear Robin,

Got it !  

Thank you so much!

0 Kudos
Reply