SPI tx interrupt is not working after rtos integration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI tx interrupt is not working after rtos integration

1,179件の閲覧回数
Embionics
Contributor III

In my project, I am using free rtos. Flash has been integrated through spi. so to test the flash and spi, I have written a test code, which was working. After that I have copied those files into my main project. Now the code is getting blocked for spi transmission interrupt. Can any one tell, is that due to free rtos settings??

 

I am attaching my code here. In Gateway_New/lib/HAL/HAL.c I have my FLASH_WRITE function which is using spi interrupt.

Original Attachment has been moved to: Gateway_New.rar

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)