SPI slave code in interrupt handler for S9S12GA240 controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI slave code in interrupt handler for S9S12GA240 controller

1,154件の閲覧回数
punithb
Contributor I

Hi All,

I am facing one more issue in gpio interrupt.

I am sending SPI data from my KEAZN64 controller(act as MASTER)  to S9S12GA240 controller.

i am sending 0x06,0xBC,0xAB data from KEAZN64 to S9S12GA240

(before sending data i am making one gpio(PP0)  high to low which is connected between both )

I am receiving data in gpio interrupt handler.

1. but if i received data in main handler there is no loss of data.

1. but if i received data in interrupt handler there is  loss of data.

Here will be interrupt and spi init code.

  /* Initialise the SPI */

    SPI1CR2 = 0x10; //8bit //0x10;             /* 8-Bit transfer width; SS pin is used by the SPI                          */

    SPI1BR  = 0x28;//0x28; //0x77;//0x77; //0x41; //0x77;             /* SPI clock = Bus Clock divided by 2048 = 15.625kHz                        */

    SPI1CR1 = 0x40; //pol,pha =0; slave mode, MSB first //0x56;             /* SPI enabled; Master mode; Active high clocks; Slave Select output enabled*/

    /* Enable Interrupt on Port P, P7 */

    //PERP =  0x03;

    //PIEP_PIEP1 = 1;

    DDRP_DDRP0=0;  // make as input

    PERP_PERP0=1; // pull up enable

    PPSP_PPSP0=0;

    PIEP_PIEP0=1;

    EnableInterrupts;  

Once i used the fallowing code in main loop , there is no loss of data.

DisplayString("IN intertttput handler   ");

   LF;

    while(rx_data[rx_cnt]!=0xAB)

    {

     while(SPI1SR_SPIF == 0);

      rx_data[rx_cnt] = SPI1DRL;

      DisplayByte(rx_data[rx_cnt]);

      LF;

      //rx_cnt++;

      //while(SPI1SR_SPTEF==0);

      //SPI1DRL = 0xBA;

                     

   }

   rx_data[rx_cnt]=0x00;

   DisplayString("End intertttput handler   ");

   LF;

i am getting all 3 data (0x06,0xBC,0xAB)

but if i used same thing in interrupt handler, i am getting only 0x06,0xAB.

means 0xBC is missing.

Here will be my interrupt handler.

#pragma CODE_SEG NON_BANKED

#pragma TRAP_PROC

void interrupt VectorNumber_Vportp PORTPP_ISR(void)

{

  

    unsigned char rx_data[12]={0},rx_cnt=0;

   interrupt_Flag = 1;

   DisplayString("IN intertttput handler   ");

   LF;

    while(rx_data[rx_cnt]!=0xAB)

    {

     while(SPI1SR_SPIF == 0);

      rx_data[rx_cnt] = SPI1DRL;

      DisplayByte(rx_data[rx_cnt]);

      LF;

      //rx_cnt++;

      //while(SPI1SR_SPTEF==0);

      //SPI1DRL = 0xBA;

                     

   }

   rx_data[rx_cnt]=0x00;

   DisplayString("End intertttput handler   ");

   LF;

   PIFP=0x01;

}

#pragma CODE_SEG DEFAULT

Could you please let me know what may the the problem?.

Thanks & Regards,
Punith B

0 件の賞賛
返信
0 返答(返信)