SPI bus example code for Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI bus example code for Kinetis

跳至解决方案
8,109 次查看
peter_fenn
Contributor V

Can any of you perhaps direct me to bare-metal SPI bus example code for Kinetis? There’s no shortage of reference for I2C but non-MQX SPI examples appear to be lacking for Kinetis (specific application context is interfacing to low-level device driver for Spansion SPI serial Flash memory)

Thanks in advance... 

0 项奖励
回复
1 解答
1,752 次查看
mjbcswitzerland
Specialist V

Hi

 

See the following: https://community.freescale.com/message/105474#105474

 

The uTasker Kinetis project contains SPI drivers for AT45DBxxx, SST25xxx and STM25(P)xxx SPI Flash (and supports simulation of them too).

 

Regards

 

Mark

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,753 次查看
mjbcswitzerland
Specialist V

Hi

 

See the following: https://community.freescale.com/message/105474#105474

 

The uTasker Kinetis project contains SPI drivers for AT45DBxxx, SST25xxx and STM25(P)xxx SPI Flash (and supports simulation of them too).

 

Regards

 

Mark

 

 

0 项奖励
回复