SPI bus example code for Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI bus example code for Kinetis

ソリューションへジャンプ
8,129件の閲覧回数
peter_fenn
Contributor V

Can any of you perhaps direct me to bare-metal SPI bus example code for Kinetis? There’s no shortage of reference for I2C but non-MQX SPI examples appear to be lacking for Kinetis (specific application context is interfacing to low-level device driver for Spansion SPI serial Flash memory)

Thanks in advance... 

0 件の賞賛
返信
1 解決策
1,772件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

See the following: https://community.freescale.com/message/105474#105474

 

The uTasker Kinetis project contains SPI drivers for AT45DBxxx, SST25xxx and STM25(P)xxx SPI Flash (and supports simulation of them too).

 

Regards

 

Mark

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,773件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

See the following: https://community.freescale.com/message/105474#105474

 

The uTasker Kinetis project contains SPI drivers for AT45DBxxx, SST25xxx and STM25(P)xxx SPI Flash (and supports simulation of them too).

 

Regards

 

Mark

 

 

0 件の賞賛
返信