SPI FIFO INITIALIZATION

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI FIFO INITIALIZATION

1,508件の閲覧回数
deepanshgoyal
Contributor I

Can anyone please give me SPI FIFO initialization .The one I have made is not working properly.I am also posting my spi fifo initialization

void spi_master_fifo_init()

{

  SIM_SCGC6 |= SIM_SCGC6_DSPI0_MASK;

  // first set the spi2_mcr

   spi_pin_mapping();

  // MASTER MODE ,Continuous clock generation, peri chip select signal, when rx data overflow overwrite the shift register, all the chip select uses high signal for deactivating, doze mode is disabled, enalbe DSPI clocks always and is not controlled by external digital pins, tx and rx are enabled  

  SPI0_MCR = ((HALT) | (MODULE_DISABLE));

  SPI0_MCR = ((TX_DISABLE)|(MASTER_MODE)|(RX_DISABLE)|(SPI_MCR_ROOE_MASK)|(SPI_MCR_CLR_TXF_MASK)|SPI_MCR_CLR_RXF_MASK|(SPI_MCR_DCONF(0x00))|(SPI_MCR_CONT_SCKE_MASK & 0x01)|(SPI_MCR_PCSIS(31)));

  SPI0_CTAR0 = (SPI_CTAR_DBR_MASK & 0x00) | (SPI_CTAR_FMSZ(0x07)) | (SPI_CTAR_PDT(0x00)) | (SPI_CTAR_BR(0x08)) | (INACTIVE_CLOCK_POLARITY_LOW) | (CLOCK_PHASE_CAPTURE_ON_LOW) | (SPI_CTAR_PBR(0x03)) | (SPI_CTAR_PCSSCK(0x02) | (SPI_CTAR_PASC(0x00)) | (SPI_CTAR_CSSCK(0x06)) | (SPI_CTAR_ASC(0)) | (SPI_CTAR_PDT(0x00)) | (SPI_CTAR_DT(0))) ; // mode 0 operation

}

BUT its not working properly.

0 件の賞賛
返信
1 返信

1,295件の閲覧回数
EarlOrlando
Senior Contributor II

Hi Deepansh,

Which MCU are you using?

Regards,

Earl.

0 件の賞賛
返信