GPIO Open-Drain I2C Bit Bang MK02FN128VFM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO Open-Drain I2C Bit Bang MK02FN128VFM

2,051件の閲覧回数
philipp_laemmle
Contributor II

Hello everybody

I want to intergrate a I2C BitBang on two of the GPIO Pins. The Kinetis processor should work as master.

Therefore I have to configure those pins as open-drain output connected with external pull up resistors.

Once the Master has send out the I2C Adress, it has to check the I2C_SDA like for the acknowledge of the slave.

The slaves gives the acknowledge by pulling the signal line low, but unfortunately when I read the GPIO with GPIO_DRV_ReadPinInput(), I get always a 0x01.

I'm a little bit confused about one sentence in the user manual of MK02FN128VFM.

The GPIO input data register

displays the logic value on each pin when the pin is configured for any digital function,

provided the corresponding Port Control and Interrupt module for that pin is enabled.

Can anybody help me to do the right configuration?

Thanks in advance.

Regards Philipp

ラベル(1)
0 件の賞賛
返信
1 返信

1,724件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Philipp,

If you connect the GPIO pin to GND are you still getting an 1 when you call the function GPIO_DRV_ReadPinInput()?

Regards,

Earl.

0 件の賞賛
返信