SPI Chip Select

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Chip Select

1,680 Views
josephchen
Contributor III

I'm using Kinetis MCUs. I wonder if it is possible to connect two SPI slave devices shared the same SS line. One of the SS lines contains a NOT logic gate so I can select the slave device by changing its GPIO value in callback function. Is it possible?

0 Kudos
Reply
1 Reply

1,445 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Joseph,

After learned your statement, I think this scenario can work out.

But I don't consider this method is good enough, I will prefer to share SPI_MISO、SPI_MOSI、SPI_SCLK pin, then use the different GPIO as the SS pin to select the external device.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------