SPI Chip Select

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI Chip Select

1,689 次查看
josephchen
Contributor III

I'm using Kinetis MCUs. I wonder if it is possible to connect two SPI slave devices shared the same SS line. One of the SS lines contains a NOT logic gate so I can select the slave device by changing its GPIO value in callback function. Is it possible?

0 项奖励
回复
1 回复

1,454 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Joseph,

After learned your statement, I think this scenario can work out.

But I don't consider this method is good enough, I will prefer to share SPI_MISO、SPI_MOSI、SPI_SCLK pin, then use the different GPIO as the SS pin to select the external device.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------