SOFTWARE IDE FOR NXP Freedom Development Platform for Kinetis® KL16 and KL26

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SOFTWARE IDE FOR NXP Freedom Development Platform for Kinetis® KL16 and KL26

ソリューションへジャンプ
4,141件の閲覧回数
BPR
Contributor I

Which IDE will be used for the NXP Freedom Development Platform for Kinetis® KL16 and KL26?

 

 
 
 
 
0 件の賞賛
返信
1 解決策
4,107件の閲覧回数
ErichStyger
Specialist I

KSDK (Kinetis SDK) and KDS (Kinetis Design Studio) and CodeWarrior is legacy, I recommend to go with the MCUXpresso IDE and SDK instead.

First there was CodeWarrior, then there was KDS, now there is MCUXpresso.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,950件の閲覧回数
stevediaz
Contributor I

Hello

For the NXP Freedom Development Platform for Kinetis® KL16 and KL26, you can use the MCUXpresso IDE, which is provided by NXP Semiconductors. MCUXpresso IDE is a comprehensive and free-of-charge development environment designed specifically for NXP's microcontrollers and microprocessors.

MCUXpresso IDE includes all the essential tools for developing, debugging, and analyzing applications for NXP's Kinetis microcontrollers, including the KL16 and KL26 series. It provides a user-friendly interface, extensive debugging features, and seamless integration with NXP's software development kits (SDKs).

You can download MCUXpresso IDE from NXP's official website, and it supports various NXP microcontrollers, making it an ideal choice for your Freedom Development Platform with KL16 and KL26 MCUs.

0 件の賞賛
返信
4,108件の閲覧回数
ErichStyger
Specialist I

KSDK (Kinetis SDK) and KDS (Kinetis Design Studio) and CodeWarrior is legacy, I recommend to go with the MCUXpresso IDE and SDK instead.

First there was CodeWarrior, then there was KDS, now there is MCUXpresso.

0 件の賞賛
返信
4,103件の閲覧回数
BPR
Contributor I
Ok, Understood. Thanks for your reply
Are both MCUXpresso IDE and SDK free? or is there any paid version depending on the code size?
0 件の賞賛
返信
4,098件の閲覧回数
ErichStyger
Specialist I

They are free of charge.

0 件の賞賛
返信
4,134件の閲覧回数
ErichStyger
Specialist I

Hi @BPR ,

not sure what you mean with 'will be used', but there is the NXP MCUXpresso SDK (https://mcuxpresso.nxp.com) for it, and you can use the SDK with a range of IDEs (I'm mostly using the MCUXpresso IDE and Visual Studio Code).

But you can use any other development environment as outlined on the MCUXpresso SDK web site.

Erich

0 件の賞賛
返信
4,109件の閲覧回数
BPR
Contributor I
Iam asking this because there are actually three IDEs
1. CodeWarrior
2. MCUXpresso
3. KDS IDE
Also, there is a KSDK and MCUXpresso SDK.
So, there is confusion for me.
0 件の賞賛
返信