S9KEAZN8AMFK RTC Wakes up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S9KEAZN8AMFK RTC Wakes up

1,134件の閲覧回数
chenhuang
Contributor II

Hi NXP FAE/AE,

   The customer only needs to use one ADC, one PWM and two GPIOs, and wake up through the S9KEAZN8AMFK RTC alarm clock after sleep. Can it be guaranteed to be within 300uA? Is there any related routine? Thank you.

 

0 件の賞賛
返信
1 返信

1,121件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @chenhuang ,

The S9KEAZN8AMFK chip has three modes: Run, Wait, Stop. If the sleep mode you mentioned is the one marked in the red box below, then it is indeed the wait mode.

Celeste_Liu_0-1736840751465.png

Please refer to the Data Sheet of it.  In the Table 4, you can see below content. They all exceed 300uA.

Celeste_Liu_1-1736840946551.png

If you're referring to the STOP (SLEEP DEEP) mode, it is below 300 μA.

Celeste_Liu_2-1736841316440.png

Hope it can help you.

BRs,

Celeste

--------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------

0 件の賞賛
返信