S9KEAZN8AMFK RTC Wakes up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S9KEAZN8AMFK RTC Wakes up

1,132 Views
chenhuang
Contributor II

Hi NXP FAE/AE,

   The customer only needs to use one ADC, one PWM and two GPIOs, and wake up through the S9KEAZN8AMFK RTC alarm clock after sleep. Can it be guaranteed to be within 300uA? Is there any related routine? Thank you.

 

0 Kudos
Reply
1 Reply

1,119 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @chenhuang ,

The S9KEAZN8AMFK chip has three modes: Run, Wait, Stop. If the sleep mode you mentioned is the one marked in the red box below, then it is indeed the wait mode.

Celeste_Liu_0-1736840751465.png

Please refer to the Data Sheet of it.  In the Table 4, you can see below content. They all exceed 300uA.

Celeste_Liu_1-1736840946551.png

If you're referring to the STOP (SLEEP DEEP) mode, it is below 300 μA.

Celeste_Liu_2-1736841316440.png

Hope it can help you.

BRs,

Celeste

--------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
--------------------------------------------------------------------------------------------------------

0 Kudos
Reply