S9KEAZN16 LIN communication project example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S9KEAZN16 LIN communication project example

1,893件の閲覧回数
cg0
Contributor II

Hello I use S9KEAZN16 as a sensor controller, and we need LIN communication, the sensor is slave node, I want to find an example, but it seems that S32DS have no example. So I want if can give me one or two examples. one is bare project without LIN stack layer. if have LIN stack, the orther one with LIN stack layer.

Thank you very much.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,800件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Aron Cheng ,

  About the S9KEAZN16 LIN examples, you can refer to the LIN stack:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW-LIN2X-J2602-D 

pastedImage_2.png

Please try it on your side.

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信