Running a K6x from external Flash via the Flexbus.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running a K6x from external Flash via the Flexbus.

779件の閲覧回数
allandimmock
Contributor I

When running a K6x from external NOR flash, should the flash interface be 16 bit or 32 bit, or can it be either? Is the K6X (thumb only) even capable of running code from 32bit external Flash memory?

ラベル(2)
0 件の賞賛
返信
1 返信

650件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Allan,

If you are using FlexBus it is able to perform 16-bit and 32-bit reads and writes using 16-bit and 32-bit interface. So, it does not matter if you use 16-bit or 32-bit interface.

Best regards,

Carlos

Technical Support Engineer