Running a K6x from external Flash via the Flexbus.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Running a K6x from external Flash via the Flexbus.

765 次查看
allandimmock
Contributor I

When running a K6x from external NOR flash, should the flash interface be 16 bit or 32 bit, or can it be either? Is the K6X (thumb only) even capable of running code from 32bit external Flash memory?

0 项奖励
回复
1 回复

636 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Allan,

If you are using FlexBus it is able to perform 16-bit and 32-bit reads and writes using 16-bit and 32-bit interface. So, it does not matter if you use 16-bit or 32-bit interface.

Best regards,

Carlos

Technical Support Engineer