Running DES-ECB with mmCAU on MKM34Z256VLL7 controller generates HardFault upon executing 'cau_des_encrypt' API.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Running DES-ECB with mmCAU on MKM34Z256VLL7 controller generates HardFault upon executing 'cau_des_encrypt' API.

1,167 次查看
shaiknisar
Contributor I

Hey Hi all,.

I'm working with MKM34Z256VLL7 controller. I have referred to the example code provided by the NXP for the mmCAU module, and i'm trying to replicate the same.

   => I'm trying to use the TDES API provided in the example code. For this i've created a new IAR Build and tried to replicate the way it is done in the example code.

   => The problem here i face is that the moment i try to execute the 'cau_des_encrypt' API it triggers 'Hard Fault'. Can someone please help me resolve this issue. I have been trying to resolve this since a week. 

NOTE: I have added the IAR Build.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,083 次查看
shaiknisar
Contributor I

Resolved the Hard fault issue.

The clock for the mmCAU module wasn't getting enabled.

0 项奖励
回复