Running DES-ECB with mmCAU on MKM34Z256VLL7 controller generates HardFault upon executing 'cau_des_encrypt' API.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running DES-ECB with mmCAU on MKM34Z256VLL7 controller generates HardFault upon executing 'cau_des_encrypt' API.

1,170件の閲覧回数
shaiknisar
Contributor I

Hey Hi all,.

I'm working with MKM34Z256VLL7 controller. I have referred to the example code provided by the NXP for the mmCAU module, and i'm trying to replicate the same.

   => I'm trying to use the TDES API provided in the example code. For this i've created a new IAR Build and tried to replicate the way it is done in the example code.

   => The problem here i face is that the moment i try to execute the 'cau_des_encrypt' API it triggers 'Hard Fault'. Can someone please help me resolve this issue. I have been trying to resolve this since a week. 

NOTE: I have added the IAR Build.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,086件の閲覧回数
shaiknisar
Contributor I

Resolved the Hard fault issue.

The clock for the mmCAU module wasn't getting enabled.

0 件の賞賛
返信