Run modes from QSPI FRDM-K82F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run modes from QSPI FRDM-K82F

4,583 Views
jozefl
Contributor II

Hi,

I'm trying to use the either normal run mode or HS run mode in my QSPI program. I've tried using the two provided functions:

BOARD_BootClockRUN and BOARD_BootClockHSRUN

My program seems to never get past these function calls when I use them in a QSPI program. If I use these functions in a program running from flash they work as expected.

Any tips on increasing the core clock speed in a QSPI program?

Thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
5 Replies

4,119 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

If you are using KSDK V2.0 QSPI example demo?


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,119 Views
jozefl
Contributor II

Yes I am using the hello_world_qspi example from KSDK_2.0 for the FRDM-K82F. Out of the box the program flashes and runs correctly from QSPI but if I add "BOARD_BootClockRUN();" immediately after "BOARD_InitPins();" then the program no longer works correctly and faults without printing "hello world".

0 Kudos
Reply

4,119 Views
konradgräfe
Contributor III

Did you find a solution to this?

0 Kudos
Reply

4,117 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

First of all, thank you for the patience.

There is a document <Kinetis Bootloader QuadSPI User's Guide.pdf> chapter 7 provide more detailed info about how to change the MCG clock mode from FEE to PEE. You also could find related demo project at KBOOT V2.0 installation path. 

I attached the <Kinetis Bootloader QuadSPI User's Guide.pdf> file for your reference.

I would recommend customer to download the KBOOT v2.0 software to get the demo code.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,117 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Sorry for the later reply.

I re-generate the same issue with [hello_world_qspi] demo.

I was checking this issue with KSDK software team.

I will let you know when there with any feedback.

Thank you for the patience.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply